As data centers evolve to support artificial intelligence, cloud computing, and high-density processing, one challenge has become impossible to ignore: heat. With rack densities climbing from 15 kW to more than 100 kW, traditional air cooling is no longer sufficient. The industry is rapidly shifting toward liquid cooling—and with it comes a need for more precise, reliable mechanical systems.
NIBCO has stepped into this space with a comprehensive portfolio of valves, fittings, and hydronic components designed specifically to support modern data center cooling. By combining proven product performance with a fully integrated system approach, NIBCO is helping contractors simplify complex installations while improving long-term reliability.
The Shift to Liquid Cooling
Liquid cooling—whether through hydronic systems or direct liquid cooling (DLC)—offers significantly higher efficiency than air-based methods. By circulating chilled water or specialized fluids directly to heat-generating components, these systems remove heat faster and more effectively.
But this efficiency depends entirely on the integrity of the system. Every valve, fitting, and connection point must perform under continuous pressure and often in chemically sensitive environments. Even minor failures can lead to downtime or costly repairs.
NIBCO products form the critical “circulatory system” of liquid-cooled data centers, ensuring consistent flow, pressure control, and system integrity throughout the cooling loop.

A Complete, Integrated Offering
One of NIBCO’s key differentiators is its ability to provide a full range of hydronic system components from a single manufacturer. This includes:
- Ball valves, including the high-performance NIBCO 585HP ball valve (rated up to 1,000 PSI)
- Butterfly valves for larger-diameter flow control
- Check valves and balancing valves for system regulation
- Strainers to protect sensitive equipment from debris
- Actuators for automated control
- Air separators to improve system efficiency
This all-in-one approach reduces the need for multiple suppliers, simplifying procurement, submittals, and coordination. It also ensures compatibility across the entire system, an important advantage in large-scale data center builds where consistency is critical.
Built for Performance and Longevity
Data center cooling systems operate continuously, often under high pressure and with specialized fluids like propylene glycol or deionized water. These conditions demand materials that resist corrosion, maintain sealing integrity, and perform over long service lives.
NIBCO meets these demands through careful material selection and engineering. Its valves and fittings are constructed from lead-free copper alloys and low-carbon stainless steel, chosen for their durability and compatibility with modern cooling fluids. The company also avoids materials prone to dezincification or stress corrosion cracking, reducing the risk of premature failure. Products like the 585HP ball valve not only offer high-pressure ratings but are also backed by extended warranties, giving contractors and owners confidence in long-term performance.

Faster Installation, Less Labor
With labor shortages affecting the construction industry, efficiency on the jobsite is more important than ever. NIBCO supports faster installation through product consistency and flexible connection options.
Contractors can choose from press, brazed, or welded connections, depending on project requirements and crew capabilities. This flexibility allows teams to optimize for speed, safety, or cost without sacrificing performance.
Additionally, NIBCO’s standardized product designs make prefabrication easier. Valve assemblies and pump modules can be built off-site with confidence that components will align correctly during installation—saving valuable time in the field.
Reducing Risk Through a Single Source Strategy
In mission-critical environments like data centers, reliability isn’t optional; it’s essential. NIBCO’s “one partner, one spec, one warranty” approach helps reduce risk by consolidating system components under a single, trusted manufacturer. This strategy minimizes compatibility issues, simplifies documentation, and ensures clear accountability if issues arise. Combined with NIBCO’s rigorous quality assurance processes, including pressure testing and precision machining, contractors can trust that every component meets performance standards before it arrives on site.
Support That Extends Beyond the Product
NIBCO’s value extends beyond its product lineup. The company provides CAD and BIM resources, helping engineers and contractors integrate components into system designs more efficiently. Its regional technical representatives and commercial sales teams offer training, troubleshooting, and on-site support throughout the project lifecycle. This level of collaboration is especially important in data center construction, where design-build coordination and rapid problem-solving are often required to keep projects on schedule.
Ready for What's Next
As data center technology continues to advance, cooling systems will only become more sophisticated. Direct-to-chip cooling and two-phase systems are already pushing the limits of thermal management, requiring even greater precision and reliability from mechanical components.
NIBCO is actively preparing for this future, engineering its valves and fittings to meet the evolving demands of next-generation cooling architectures. With continued investment in research and U.S.-based manufacturing, the company is well-positioned to support the next wave of data center innovation.
A Partner in Performance
For mechanical contractors, building data centers today means navigating tighter timelines, higher expectations, and increasingly complex systems. Success depends on more than just individual components; it requires a comprehensive, reliable solution backed by expert support.
NIBCO delivers exactly that. With a complete lineup of products combined with deep hydronic expertise, NIBCO simplifies building high-performance cooling systems. In an industry where uptime is everything, NIBCO stands out as a partner contractors can trust, helping turn the challenges of modern data center cooling into opportunities for smarter, more reliable construction.